Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF01SA - Setting the IP Address

Posted on October 04, 2017 at 14:34Hi,I have recently just started working on Wi-Fi code on the SPWF01SA module using the STM32F1 Nucleo Development Board.I was able to get the various configuration values from the Wi-Fi module using the functions b...

0690X00000608TUQAY.png 0690X00000608N9QAI.png

SPI2 not working in stm32f070

Posted on October 04, 2017 at 07:37Hello Allcurrently i am working in Fatfs with stm32f070 with spi1. when i move to spi2 its not working. i am trying multiple times but i cant get success. here is my init functionvoid SPIFlashInit(void) { SPI_InitT...

Build OTA in Sigfox project on BlueNRG1

Posted on October 02, 2017 at 04:56Hi,I tried to add OTA function in BLE_SigFox_SensorDemo project,and according to OTA guide, I have to add, ST_OTA_LOWER_APPLICATION=1 or ST_OTA_HIGHER_APPLICATION=1 as preprocessor and linker options.After adding S...

Wei Lu by Associate
  • 765 Views
  • 0 replies
  • 0 kudos

A few questions about BLUENRG-MSCSP

Posted on September 28, 2017 at 09:49Hello. I have got a few questions about  BLUENRG-MSCSP. Could you help me? 1. What par of an inductor you recommend ( Power management strategy using step-down DC-DC converter )? What par of a capacitor  you reco...

STM32L476JEY BootLoader after FOTA

Posted on September 27, 2017 at 15:57In my program i'm doing FOTA via BLE.I developed my code with Nucleo-l476RG EVB and Nucleo-IDB05A1, based on the FP-SNS-FLIGHT1 program.Now I'm working with my custom PCB using STM32L476JEY as MCU and BlueNRG-MS ...

0690X00000608HAQAY.png

SPWF04SC

Posted on September 25, 2017 at 14:56I use Altium Designer to create my PCB, and so i need  the 3D step of the SPWF04SC.Somebody, could send it me?Best regards#spwf04sc-3d-step-model #3d-step-model

wifi bootloaders for SPWF04SA

Posted on September 25, 2017 at 11:15Does STM wifi module SPWF04SA comes with inbuilt Wifi-bootloaders ? If not does someone has hints on designing the wifi bootloaders ?#wifi-module #spwf04sa

STiH416 modules or evolution kit

Posted on September 25, 2017 at 09:35I want to find a video encoder modules using STiH416 for my project. Can anyone suggest me some names and documentations of them?Thank you very much.#stih416 #video-encoder

thuan vu by Associate
  • 561 Views
  • 0 replies
  • 0 kudos