cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF04 SPI ISSUES

Andrew Smit
Associate
Posted on July 12, 2017 at 09:32

We are using the SPWF04 SPI and have the following issues

1) No Ack after TCP socket data packet sent:

I can setup a client socket or a server socket and start streaming data but at some point the SPWF04S does not ack and 20 seconds later the module resets. (This 'lockup' is random and can be from a few seconds to 2 minutes)

There is no ack interrupt from the module

We have tried to send differnt sized packets (512 to 3k, with same 'lockup'

2) A UDP server socket is opened and the data received via the WIND 55 process. My problem is that 30% of the messages have a faulty byte in the message, i.e. �{\'TimeRequest\'}' or '{\'TimeR quest\'}'. If the first byte is incorrect it is always a 0x80 �� � but the byte that is incorrect in the message is always a 0xFF

3) How do I reply to a UDP broadcast received on the UDP server socket? If I send a reply via the current socket I don�t receive it on the remote side.

#spwf04 #spi
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0