cancel
Showing results for 
Search instead for 
Did you mean: 

Build OTA in Sigfox project on BlueNRG1

Wei Lu
Associate

Posted on October 02, 2017 at 04:56

Hi,

I tried to add OTA function in BLE_SigFox_SensorDemo project,

and according to OTA guide, I have to add, ST_OTA_LOWER_APPLICATION=1 or ST_OTA_HIGHER_APPLICATION=1 as preprocessor and linker options.

After adding 

ST_OTA_HIGHER_APPLICATION=1 in linker options,

IAR shows error message LP011, which represents setion placement failed.

Can someone help me here? Thanks.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0