Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BlueNRG-MS v7.2c Central is not receiving ADV_IND & SCAN_RSP > 18 bytes - why it cannot receive up to MAX_ADV_DATA_LEN?

Posted on May 12, 2018 at 05:47Hello - wrt the maximum total size of a BLE advertisement or scan response of 31 bytes:The BlueNRG-MS v7.2c Peripheral can generate either at max expected length.But when I run the BlueNRG-MS v7.2c Central, if the tota...

SPBTLE-1S SPI_IRQ pin?

Posted on April 25, 2018 at 11:18Hello, I want to make a PCB with a microcontroller STM32L476RG and a Bluetooth module SPBTLE-1S. I plan to use the SPI for the communication beetween the microcontroller and the BLE module but I don't know which pin ...

SPWF04 Configuration Failure:4

Posted on May 15, 2018 at 15:18On one of my boards that use the SPWF04 module I have started to see Win7: Configuration Failure:4 which from the manual indicates the RTC cannot be initialised.For these errors my approach was to hold the device in re...

S2-LP I/Q data GPIO pins

Posted on February 13, 2018 at 14:49Hi,I have a question about the STEVAL-FKI868V1 development kit that is based on the S2-LP sub 1GHz transceiver. We have a system that works at 868MHz and the signal that commes from the system is fed into multiple...

BlueNRG BLE stack port

Posted on May 11, 2018 at 07:37Is it possible to use BlurNRG BLE stack in STM32F103 CPU and use UART as a HCI interface to any Bluetooth chip?Read through BlueNRG manuals and those looks like BlueNRG is ment to be used only in SoC and ACI layer betw...