Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do i limit the channels that will be used in the STM32CubeExpansion_LRWAN_V1.2.1 End Node example

I am using a B-L072Z-LRWAN1 and the STM32CubeExpansion_LRWAN_V1.2.1 End node example with an 8 channel lora gateway set to channels 1-8. The gateway is receiving some data from the End Node. Appears the End Node may be transmitting on channels that t...

Resolved! S2-LP Custom Board - Need help

Posted on January 07, 2018 at 03:35 Hi I have my custom RF board using S2-LP and balunBALF-SPI2-01D3 ( /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fdatasheet%2Fgroup3%2Fe9%2Fff%2Fcd%2F1e%2F4...

Resolved! How get best performance from BlueNRG-X on scan mode?

Hi, I'm using the example "BLE_SensorDemo_Central" from SDK to design a PoC to scan iBeacons devices.I can't figure out why the scan procedure is too slow. I have two iBeacon devices near by the BlueNRG-1. They are sending iBeacon messages in 3Hz, bu...

uilter by Senior
  • 1330 Views
  • 5 replies
  • 0 kudos

BluNRG-1. LowPowerMode.

Hi All!I have a next question for low power mode.When i have using low power mode - SLEEPMODE_WAKETIMER - GPIO has generate some impulse for fix T-period. This reason in of operation low power mode?GPIO_SetBits(GPIO_Pin_6); HAL_VTimerStart_ms(0,2000)...

zovkorall by Associate II
  • 1169 Views
  • 2 replies
  • 0 kudos