Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there a limit to the number of characteristics in the BlueNRG-1, and is it dependent on UUID length?

I wrote a version with 16 bit UUIDs, but it seems that LightBlue doesn't handle duplicate UUIDs in the same service (Service: Automation I/O; I added 4 analogs and 3 digitals; some are R/O and some are R/W, but LightBlue only is using the permissions...

TJohn.14 by Associate II
  • 711 Views
  • 0 replies
  • 0 kudos

Unable to Flash the Firmware in BlueNRG-1

Hi Sir,Greetings of the day,Here, I am using the BlueNRG-1 development boards. I downloaded the SDK from the st.com. I am getting an error message as follows while flashing. I am using st-link /v2 to flash. Please help me.Regards,

0690X00000AA05LQAT.png
GShai by Associate II
  • 1038 Views
  • 1 replies
  • 0 kudos

Resolved! BlueNRG-2 in STM32CubeMX

Hi,Greetings of the day,Here I am searching the BlueNRG-2 in the stm32cubemx. But I am unable to found out that. Please help me Regards,

GShai by Associate II
  • 1287 Views
  • 1 replies
  • 0 kudos

How can i get the MAC adress of the blueNRG-2 ?

Hi , Object: Establish a BLE connection between the BlueNRG-2 and mobile phone app . I'm using BlueNRG-2 on STEVAL-IDB008V2 that i want to configure it as a network coprocessor via SPI mode with nucleo-L053 board.  For now : -I developped the applica...

IGhao by Associate II
  • 726 Views
  • 0 replies
  • 0 kudos

I am trying to replicate SDK_BasicGeneric_A example transmitter code on my custom board. And it works well only after I set BYPASS_LDO to 1. What is the reason of such behavior?

Processor is PIC16LF18446, interface with s2lp works fine. I use S2LP_Library from SDK 1.2.1 with some adaptations for PIC. Three boards with the same behavior - possibility of soldering error is minimal. Frequency 433 MHz, crystal 50 MHz.

IShug by Associate
  • 977 Views
  • 1 replies
  • 1 kudos