Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FOTA with IoT kit discovery node

I'm trying to get basic FOTA working with the example binary from en.fp-cld-azure download (Azure_IoTCentral_BL.bin).I have the example binary loaded on the board and successfully connecting and communicating with my Azure IoT Central app.I added the...

DSabo by Associate III
  • 667 Views
  • 0 replies
  • 0 kudos

Bluetooth 5 module with ST32

Hello,I'm designing a custom PCB with STM32L476RG. I need to add Bluetooth 5 connectivity. I'm looking for a BT module with the following requirements:Transmit at least 2MbpsAs small as possibleIt would be great if it will come with code exampleI don...

Unicleo does not work with Sensortile

Hi, I tried to read Sensortile data with Unicleo but I found some issues. Basically I can connect sensortile with unicleo but when press the button "start", or nothing happen, or the communication begins, but after 20/30 seconds Unicleo stops to read...

We are working on design that would use the STUSB4500L in an all +5V system. The host processor is also at +5V. Unfortunately the STUSB4500L list +4.5V as recommended operating levels for the IO. What would would be risk of operating at +5V IO.

We are working on design that would use the STUSB4500L in an all +5V system. The host processor is also at +5V. Unfortunately the STUSB4500L list +4.5V as recommended operating levels for the IO. What would be the risk of using the outputs and I2C in...

JMart.21 by Associate
  • 569 Views
  • 0 replies
  • 0 kudos