User Activity

Hello everyone,I'm trying to use a KSZ8863 to monitor ethernet traffic. the KSZ8863 is connected to a STM32F767 via RMII.Im using the STMcubeIDE lwIP stack.I have no problem getting a ip-adress and ping the STM32. Also the SMI interface to the KSZ se...
Hello there :)I'm trying to use a KSZ8863 Ethernet PHY with the STM32F767. I'm using the Nucleo F767ZI Board where i unsoldered the jumpers to the onbord PHY. The KSZ8863 is then connected via the Morpho connectors.I just used the Code generated by t...