Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to debug Teseo liv3F RF or liv3F configuration issue, I am using a TESEO liv3F in my design, connected by uart with my stm32L0, the communication works but the system doesn't find any satellites. How can I debug this issue by using the UART com ?

The Teseo's firmware hasn't changed (factory's version). The RF design is the same has the strkt01 design, but my board doesn't find any satellites, GPS and Galileo are activated, I used a GNS1A1 board with the same antenna, I set GPS and Galileo con...

Kprac.1 by Associate
  • 773 Views
  • 0 replies
  • 0 kudos

IODD files for STEVAL-IDP003V1 (IO-link device)

Hi all,I have purchased the evaluation kit STEVAL-IDP003V1 (IO-Link device) and want to test it with a master of Siemens (it supports both versions). But I need the IODD files for the master configuration and can't find it anywhere. I already tried ...

Luis1 by Associate
  • 752 Views
  • 0 replies
  • 0 kudos

Hi All, I'm using STUSB4500 as USB Type C PD controller. When am connecting type C cable from adapter to the board it is able to power up. But when I remove the cable and connect again it is not powering up.

For the next time I have to re-connect the adapter than re-connecting type C cable for powering the board. Please help me to find a solution for this issue.Regards,Vyshnav Krishnan

Vvk.755 by Associate II
  • 3290 Views
  • 8 replies
  • 0 kudos

STML011K4 Stopmode consumes too much current.

Hello,Running my program on the STML011k4 consumes about 50mA, when in stopmode this drops down to about 40 mA. I know the stopmode does still power the RAM, but 40mA is way too high according to the datasheet. Another thing I find odd is that the LE...

SPlat.1 by Associate
  • 644 Views
  • 0 replies
  • 0 kudos