Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is BLUENRG-M2 module need firmware upgrade?

HiI am using bluenrg M2 module, bluenrg_m2sa and it's expansion board x_nucleo_bnrg2a1.Module with expansion board is working but module purchased separately is not. As mentioned in the errata sheet of expansion board do I need to update every new ...

Skada.3 by Associate III
  • 1571 Views
  • 2 replies
  • 0 kudos

Which one of the "BLE" or "Wi-Fi 802.15.4" is more fit (and suitable) in order to using into the smart wireless network including many sensors.

HelloWe would like to know that, which one of the "BLE" or "Wi-Fi 802.15.4" is more fit (and suitable) in order to using into the smart wireless network including many sensors (when there are more than 4 sensors in the network).Thanks

ST25R3912 calibration

Hi, I'm new with the NFC family. I am have issue with calibration for ST25R3912. I have been read the document but not found any idea. Can anyone give me the suggest to help me calibration for ST25R3912 . Thanks.

TTran.6 by Associate
  • 522 Views
  • 0 replies
  • 0 kudos

BlueNRG 2N - link status function returns 255

I have BlueNrg2N chip in advertising mode and I sometimes have a situation that chip stops advertising on it own and aci_hal_link_status function returns 255 (all status bits are set). Maybe someone have any idea what does it mean and why it happens.

DJędr.1 by Associate
  • 445 Views
  • 0 replies
  • 0 kudos

Is the STUSB4710 VBUS enable mandatory?

HiIs it possible to use the STUSB4710 without the VBUS_EN_SRC switch? In such a way the the VBUS is always sourced from the supply side.I expected this to work, but when I tried it on the STUSB4710A evaluation module, it seems it will not set any PDO...

TNils.1 by Associate II
  • 683 Views
  • 1 replies
  • 0 kudos

STUSB-4710 in STEVAL-ISC004V1 toggling VBus_EN_SRC

Hello,I just got a STEVAL-ISC004V1 kit for evaluating the STUSB-4710 in a USB-PD Application.As described in the manual I connected it to a 24V power supply and connected it to the Nucleo F072RB and the corresponding GUI. I can access the device and ...

LB1 by Associate
  • 786 Views
  • 1 replies
  • 0 kudos