cancel
Showing results for 
Search instead for 
Did you mean: 

USI STM32 Nucleo expansion board for LoRa

SRavn.1
Associate II

Hi,

Bought the STM32 Nucleo kit w. USI Lora shield.

Disappointed when I found out that the documentation wasn't that great.

When using AT_Master or the End_Node example I dont find any options for retrieving the debug data.... Is the only option I have to spy on the TX/RX on the shield itself?

Or is it possible to retrieve the debug messages that is already in the examples?

BR,

Sindre

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

The USI module is a third-party implementation, with closed source.

An SWD header can be fitted, and the firmware can be replaced with relatively little porting effort. You can program/debug via an external ST-LINK attached to the header.

Not sure the USI module provides any additional diagnostic/debug information, review their data sheets and manuals.

For a richer experience I'd recommend the Discovery Board with the Murata module. It has a larger FLASH memory, and a newer radio chip, and would allow you to add as much diagnostic and telemetry as you need. Can support several UART and I2C

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
SRavn.1
Associate II

Wow @Community member​ ,

Fast answer :)

Ok, yeah I was ordering the wrong kit.

For some reason I believed that my order was with the MBed Lora shield not the USI one...

**** happens.

Thank you