cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LPQTR with external power 1.8V on SMPS2.

rraf3
Associate

Hi all!

I developed custom board with S2-LPQTR and STM32 uc.

S2-LPQTR - answer through SPI and transmite to radio channel through BALF-SPI2-02D3, but don't receive any message.

I connect on SMPS2 pin external 1.8V from LDO.

In all example boards internal SMPS used and all examples use this line of code:

(S2-LP_DK_1.3.1) //this macro sets the SMPS switching frequency to 3.12MHz.

#define S2LPCmdStrobeRx()         {uint8_t tmp=0x90; S2LPSpiWriteRegisters(0x76,1,&tmp);\

                                    FEM_Operation(FEM_RX); S2LPCmdStrobeCommand(CMD_RX);}

#define S2LP_CMD_StrobeRx()       {uint8_t tmp=0x90;\

(en.x-cube-subg2) S2LP_ConfigRangeExt(PA_RX,S2LP_ManagementGetRangeExtender());\

S2LP_WriteRegister(0x76,1,&tmp);\

                    S2LP_CMD_StrobeCommand(CMD_RX);}

In tthe datasheet of S2-LP writed:

"The SMPS output voltage can be controlled in TX only or for both RX and TX according to

the SMPS_LVL_MODE bit of the PM_CONF1 register.

 1: SMPS output level will depend upon the value in PM_CONFIG register just in TX

state, while in RX state it will be fixed to 1.4 V.

 0: SMPS output level will depend upon the value written in the PM_CONFIG0 register

(SET_SMPS_LEVEL field) both in RX and TX state."

What i need to write S2LPCmdStrobeRx() in don't used SMPS? (with external 1.8V )

Thank all!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0