Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

St ble NRG2 (BLUENRG-M2SP) : reading the characteristic issue : hi Every one i using BLUENRG-M2SP chip , i using st ble sensor app to communicate the chip , the problem statement , AS below

1. if i read and write  characteristic in the service  its working fine if write one characteristic and read on other characteristic of same service , its not working . after that its not able to reconnect , during this scenario i need to restart ...

mkuma.1 by Associate II
  • 4974 Views
  • 11 replies
  • 0 kudos

Hi, I'm interfacing Nucleo-L476RG with a UART Device. If I power off that devices, my Nucleo code freeze and I need to manually reset it. I need to power-on and to power-off the device and the Nucleo must continue to works.

Nucleo send through UART4 and receive with DMA from devices. Then Nucleo send to PC via USART2 for debugging. In UART4 there is Idle Line detect for receiving unknown length of data.This is my code: MX_GPIO_Init(); MX_DMA_Init(); MX_UART4_In...

FManc.1 by Associate II
  • 825 Views
  • 0 replies
  • 0 kudos

St ble NRG2 (BLUENRG-M2SP) : reading the characteristic issue : hi Every one i using BLUENRG-M2SP chip , i using st ble sensor app to communicate the chip , the problem statement , AS below

1. if i read and write characteristic in the service its working fineif write one characteristic and read on other characteristic of same service , its not working . after that its not able to reconnect , during this scenario i need to restart ble ch...

mkuma.1 by Associate II
  • 812 Views
  • 0 replies
  • 0 kudos