Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm using the "SampleApp" and "Beacon" BlueNRG demos. I have one master and two slaves. The two salves should be in sleep mode except when they send data. I need data transmission every 50ms on each slaves. What is the best way or example to achieve it?

We need to have as most is possible a constant communication between the master (data receiver) and the two slaves (data senders). The data sent by each slaves should be around from every 20ms to 100ms. So the receiver would receive data every 10ms t...

SGren.1 by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

Can STOTG04ES Exposed pad connected to Ground?

Dear Sir/Madam,I have selected STOTG04ES as replacement for ISP1301BS. Major difference that I could find is the Exposed pad in both ICs. In ISP1301BS should be connected to ground but in STOTG04ES it is NC. Kindly clarify that on connecting to GND ...

B-072Z-LRWAN ACK

Hello,I am using the evaluation board B-072Z-LRWAN with the example code provided by ST (STM32CubeExpansion_LRWAN_V1.3.1), the End Node project. Data is received on my LoRa server, messages are sent as "Unconfirmed". Now, I want to send "Confirmed" m...

0693W000000WVZ6QAO.jpg 0693W000000WVYrQAO.jpg 0693W000000WVYDQA4.jpg
emil28 by Senior
  • 1455 Views
  • 1 replies
  • 1 kudos