cancel
Showing results for 
Search instead for 
Did you mean: 

file transfer with BLE

a28j
Associate II

Hi, I use a X-NUCLEO-BNRG2A1 with a NUCLEO-L476RG .

I want to transfer a file (a driver) with the BLE, is it possible?

Or does the X-NUCLEO-BNRG2A1 allow the use of bluetooth BR / EDR to transmit files with the OPP profile?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

It is possible to transfer a file over BLE. Transferring data is one of the main functions of BLE actually.

X-NUCLEO-BNRG2A1 (BlueNRG-M2SP based) is a BLE only expansion board, which means it doesn't support BR/EDR nor classic profiles such as OPP.