Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Lora node ns1 AT master

Hi everyone, I have a p-nucleo lorawan 3 kit with a nucleo-l073rz board and a lorawan ns1 lora board. ​I'm trying to setup the AT master example from I-NUCLEO-LRWAN addon using keil uvision. I uploaded the program and activated the CMD_DEBUG but I do...

PDevo.1 by Associate II
  • 2848 Views
  • 4 replies
  • 0 kudos

Custom board with SPBTLE-RF0 module using the X-CUBE_BLE1 software package initialises and advertises to mobile phones but connecting to device fails with Error 133 (0x85): GATT ERROR?

Hi,We are currently working on a custom board with the SPBTLE-RF0 used for BLE communication and a uC from the L4 family (STM32L4A6VGT6P). We used the SensorDemoBLE example as a starting point and programmed it to the board through SWD. From adding b...

0693W00000GWwbDQAT.png
Jf.1 by Associate II
  • 811 Views
  • 0 replies
  • 0 kudos

I2C with Melexis 90640

I am developing a hardware using as a board a Nucleo 144 to which I have to connect via I2C (pins set via stmcubeMX) a Melexis 90640 thermal scanner, I am experiencing problems with communication or rather, I struggle to understand the logic of readi...

Icont.1 by Associate II
  • 2892 Views
  • 7 replies
  • 0 kudos

Resolved! FDCAN configuration on STM32U575

I need to use FDCAN to send CAN messages. Since I want to receive each message (without filters) I do this :sFilterConfig.IdType = FDCAN_STANDARD_ID; sFilterConfig.FilterIndex = 0; sFilterConfig.FilterType = FDCAN_FILTER_DUAL; sFilterConfig.FilterCon...

CSou.1 by Associate II
  • 2676 Views
  • 2 replies
  • 0 kudos