I am trying to program an STM32F103C8T6 over USART via the System Memory Bootloader. I've already tried with PL2023 and FTDI FTR232RL based USB-TTL converters. I've tried with multiple computers and multiple tools provided by ST. Also, I tried jumpin...
HiIt's just that something strange happened to meIf I use RKit-ARM 1.68.18.0108 I get the following CheckSum "D9D0460"But if I upgrade RKit-ARM to 1.72.19.0253, there will be a version error problemBut 1.72.19.0253 is to fix the problem of CheckSum d...
HiThe command to download our firmware is as follow (with the option bytes display to show that protection is disabled):STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -ob displ -e all -d C:\Temp\cu.hex -d C:\Temp\data.hex -v -rstThe result always ...
Hi all, I am new at STM32 world, however I had a 1-2 days long meeting with Bluepill board about two years ago. That time I used succesfully Atollic studio to do my first steps with Bluepill and ST-LINK clone bought on ebay. Now I want to re-start wi...
Hello there,I am working on a project. In the project I want to implement, an external ADC module will collect the data and transfer it to the STM32F103C8. My STM32F103C8 microprocessor will transfer these data to my wireless module. Here I am having...
I am "Learning" assembly, So I have tried to program my stm32f103 in assembly (a simple program to blink a led). The problem is that the program runs when uploaded using st-flash utility. But, If I press reset button, the program stops working.Here a...
Hello everyone,I have a PCB with an embedded STM32F103 on it. The PCB provides access to some ports on the side. Those are linked to VDD, PA9, PA10, PA13, PA14 and GND. I tried connecting to it with Cube Programmer using a FT232RL as pictured below :...
Hi everybody. I am using uart dtr and rts pin to connect stm32f103c8's boot0 and nrst pin. İf I could set those pin when update mcu firmware, In this manner I can programming mcu without any touch to reset or jumper. Can someone give me a solution?
I'm using STMCubeProgrammer for program STM32F103 MCU. But I don't have any access to MCU RESET PIN. So I enter to BOOT Mode by source code in my application, But when I want to turn back to application from boot mode the "Run After Programming" opti...