User Activity

Heyin a project of us we are using the legacy STMFlashLoader to flash firmware on a STM32F103 via the system bootloader on UART1, but wanted to migrate to STM32CubeProgrammer now. In this application the PC (Win10) which runs STMFlashLoader/STM32Cube...
I have a project which uses SPI DMA, and the SPI DMA appears to fail when I enable the instruction cache (ICache! not DCache), but otherwise appears to work perfectly fine. I do observe this for both a F722ZE and G491RE.I'm working on this since 3 we...
I know I'm not the first reporting such an issue here, but the "solutions" in the previous threads did not help.I yesterday have installed STM32CubeIDE 1.7.0 using the installer. When trying to run a code, a dialog opens saying "No ST-LINK detected!...
Posted on October 05, 2013 at 11:08Hey Everyone Using a http://www.mikrocontroller.net/part/STM32F103RB I want to use Tim2 and Tim3 for generating a PWM, and want to start them both together such that they run prefectly in sync. Unfortunately, this ...
Kudos from