STM32 MCUs Security

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5 TF-M Crypto services - AES GCM DPA-protected

Hi,I am using the X-CUBE-AZURE example with the B-U585I-IOT02A development board equipped with STM32U5 microcontroller.Reading the tfm_mbedcrypto_config.h file of the TF-m it says that AES GCM is available with protection against DPA attaccks but in ...

Domenico by Associate III
  • 517 Views
  • 2 replies
  • 0 kudos

Application hangs when doing a remote update

The details of this project are like this. I have a working product on the F417 that I wish to add Remote update capabilities to.Product is already deployed with SBSFU and updates using Ymodem through the UART work fine.What I am trying to add on now...

Eugene G by Associate II
  • 483 Views
  • 2 replies
  • 0 kudos

Resolved! Cannot debug the AWS demo on B-L475E-IOT01A1

Dear all,For an IoT project I would like to run the demo of the AWS package provided by ST but for some reason I could not manage to debug the demo project.To do so I have downloaded the X-CUBE-AWS_v2.0.0 package and used the following ressources : S...

VSpad.1 by Associate II
  • 908 Views
  • 7 replies
  • 0 kudos

I am learning about X-CUBE-AWS examples, when update from OTA, I get a SIGNATURE CHECK FAILED exception, somebody can help me to resolve this problem?

I download X-CUBE-AWS 1.4.0 to compile and install on my STM32F769IDISCOVERY board, everything running ok, but when I configure it to update new app version from OTA, after reboot is shows:= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL= [SBOOT] ST...

saico by Associate II
  • 368 Views
  • 2 replies
  • 1 kudos