STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! How to remove a custom External Loader

Hello,I renamed my custom external loader and now STM32CubeProgrammer gives an error each time I launch it. The new external loader is loaded without problems but I keep getting this error. Is there a way to clean the list of expected external loader...

External loader for the SST26VF064B Flash Memory

Hello Everyone,I'm working on the Mikromedia 7 Capacitive board and I'd like to store my fonts and images in my external Flash Memory, the SST26VF064B. I searched in /bin/ExternalLoader and there is no example for this Flash.So I decided to make my o...

0693W00000D2b3hQAB.png 0693W00000D2b3wQAB.png
MLair.1 by Associate III
  • 7373 Views
  • 13 replies
  • 0 kudos

STM32CubeProgrammer on Apple Silicon

Has anyone experienced issues trying to run STM32CubeProgrammer on Apple Silicon, and overcome them?I am trying to use it to flash to an STM32F103 micro, but the flashing fails partway through.The issue reproduces using the CLI version of STM32CubePr...

apullin by Associate II
  • 3649 Views
  • 3 replies
  • 0 kudos

Resolved! External QSPI Loader data read failed message

Hello,I followed the STMicro YouTube tutorial for developing an external QSPI loader. I am using the W25Q128 attached to the NUCLEO-H7A3ZI-Q. The flash is working fine with my driver using the test program "main_test.c" provided with the tutorial, an...

DWWelch by Associate III
  • 8552 Views
  • 11 replies
  • 4 kudos

STMCubeProgrammer FUS/Stack upgrade with USB bootloader

While reading the UM2237 (STM32CubeProgrammer software description - User manual) data, I came up with a question.The FUS/Stack upgrade order is explained in Table of Contents 2.7 Flash the co-processor binary using graphical interface. Do I have to ...

dami_0-1691717888375.png
dami by Associate
  • 1200 Views
  • 0 replies
  • 0 kudos

Resolved! SPI MOSI and SCK pulses on oscilloscope

When I try to communicate my STM32L4P5-DK through SPI protocol. I fed the MOSI and SCK pin to the oscilloscope and checked the output there I got several doubts1) when I send a data 0xAA to the slave ( HAl_SPI_Transmit(&hspi2,0xAA,1,10) ) with the ba...

0xAA.jpeg 0xAA_.jpeg 0xFF.jpeg
ajimathew by Associate III
  • 4797 Views
  • 4 replies
  • 4 kudos