STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer - write to memory without reset

Hi,I want to write U32 value to EEPROM (STM32L07) without resetting after writing is done. 1) This writes the value, but then resets the MCU: STM32_Programmer_CLI.exe -c port=SWD mode=normal freq=8000 -w32 0x8080000 0x3 -v 2) I tried this: STM32_Prog...

JR2963 by Senior II
  • 1237 Views
  • 1 replies
  • 0 kudos

stm32wb10 update problem.

Need Assistance with Updating STM32WB10 - Seeking Help!Hello Everyone,I hope you're doing well. I'm currently facing a bit of a challenge and could use some guidance from the STM32 community. I'm attempting to update my STM32WB10, but I'm encounterin...

SMazu3_0-1694442778986.png
SMazu.3 by Associate III
  • 2186 Views
  • 4 replies
  • 0 kudos

Resolved! RTC initialization with STM32CubeProgrammer

Hello Community,Is it possible to initialize and start the Real Time Clock (RTC) of the STM32U585 at the same time as the firmware and Option Bytes are installed into the MCU with STM32CubeProgrammer SFI process?

ELuca.2 by Associate II
  • 1495 Views
  • 1 replies
  • 0 kudos

programming flash bank 2 sometimes fails with cli

I am using STM32CubeProgrammer (2.14.0) on Linux/Ubuntu 22.04 with NUCLEO-H563ZI.I do not observe any problem when I use the GUI application but I would like to use the CLI.I do not observe any issue when I write/download a program (elf or bin) to ba...

mete by Senior II
  • 1797 Views
  • 2 replies
  • 0 kudos

Resolved! STM32Cube Programmer Version 2.13.0

Dear ST Community, I would like to address an issue we have encountered while flashing the program on the STM32L562VETb microcontroller using different versions of the STM32 CubeProgrammer software. Our observations indicate a significant performance...

Kavan by Associate II
  • 5477 Views
  • 5 replies
  • 0 kudos