STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32F769I-DISCO, MB1225 B-02, A201800875

Hi,I have another problem with the board "STM32F769I-DISCO, MB1225 B-02, A201800875".I wanted to restore the original firmware of the board.Download from ST site the image "10_2020\32F769IDISCOVERY_demo\Binary\STM32769I-DISCO_DEMO_V1.0.0_FULL.hex". L...

DShub.1 by Associate II
  • 3668 Views
  • 5 replies
  • 0 kudos

Regarding_ST_LINK

Hai ST, I am working "STM32f103c8t6", while connecting st link debugger  , shows like   "UR connection mode is defined with the HWrst reset mode" ... 

RAJAVELU by Associate
  • 1050 Views
  • 1 replies
  • 0 kudos

Resolved! API from STM32CubeProgrammer 2.14.0

Hello,I have seen that in the new version of STM32CubeProgrammer (v 2.14.0) there's a new API that can be used to program a flash using DFU bootloader (API which I didn't see in my previous STM32CubeProgrammer).In addition to the writeMemory() now we...

FValm1_0-1696406898788.png FValm1_1-1696406931297.png
FValm.1 by Associate III
  • 3283 Views
  • 4 replies
  • 0 kudos

Resolved! Write Protection (WRP) STM32G4xx

WRP cho phép cấu hình các vùng bộ nhớ Flash không thể ghi vào sau khi chúng đã bị khóa. Lõi xử lý chính (Cortex-M4) chỉ có quyền truy cập và thực thi mã nguồn trong các vùng bộ nhớ được bảo vệ bởi WRP??? Điều này đúng hay sai?