STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! External flash nucleo-F746ZG with w25q128jv

Hello, I have a problem when i try to load a bin file using External flash. I created my own external flash with w25q128vj and nucleo F746ZG .When i try to load a bin file with stm32programmer its work only if the bin file is smaller than 128kb. Some...

Stlinkos by Associate II
  • 4464 Views
  • 7 replies
  • 1 kudos

DEV_TARGET_HELD_UNDER_RESET error from ST-LINK

I'm a complete newbe at directly programming STM and am learning using a Nucleo-l476RG board. When I try and run my code from STMCubeIDE I get errors failed to execute MI command and then "the system tried to join a drive to a directory on a joined d...

G0MGX by Associate
  • 15672 Views
  • 9 replies
  • 3 kudos

Resolved! How to use external loader from Visual Studio Code

Hello,I have a project that need external loader for QSPI Flash (STM32F412G-Disco board).I'm using Visual Studio Code to write code and build the project. It work fine and i can load it with STM32CubeProgrammer.For other project, without External Loa...

ANauz.1 by Senior II
  • 3613 Views
  • 2 replies
  • 0 kudos

Problem with program not starting after reset

Hello.I am experiencing the following problem during development with STM32L4A6VGTxP.Is there any solution?[Configuration.]Custom board with STM32L4A6VGTxP microcontrollerSTM32CubeIDE v1.9.0STM32CubeProgrammer v2.13.0Firmware package STM32Cude FW_L4 ...

ma-hara by Associate II
  • 1385 Views
  • 0 replies
  • 0 kudos

Resolved! can't update STM32 Cube Programmer

Hi,when starting STM32 Cube Programmer (W64) or checking for updates I get this messageThere is "No Proxy" set in the Proxy settings and the Windows PC has internet access (browsing www works).Any ideas?Thanks,M

mha_0-1697473614723.png
mha by Associate
  • 10041 Views
  • 12 replies
  • 11 kudos

M29W128GL_STM32H7B3I-EVAL.stldr

HiIs it possible to get the Source code and project files?For the external Flash loader “M29W128GL_STM32H7B3I-EVAL.stldr”Used in the STM32CubeProgrammer.Best regardsStig

SKris.4 by Associate II
  • 852 Views
  • 0 replies
  • 1 kudos