STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Stm32CubeProgrammer file differences

 Hello everyone,I have a .hex and a .bin file that set an output to high/low on an STM32H745.When I upload the .hex file, my project works correctly, but when I upload the .bin file, it doesn't work.I'm sharing both files.I can't figure out what I'm ...

Matt_ by Associate II
  • 1744 Views
  • 4 replies
  • 2 kudos

Resolved! Error: No STM32 target found! (SMT32N657X0-Q)

Dear Community Teams, My name is Cong, and who currently perform projects with smt32. However, there is one error that I need advice from you if possible.The description of the error as below:- Environment used: Windows 10- Board: SMT32N657X0-Q- Tool...

01_connect_laptop_port.JPG 02_resetmode_Software_Not_connect.JPG 03_Hardware_reset_connected.JPG 04_Cannot_See_ROT_Provitioning_SMT32N657X0-Q.JPG

STM32CubeProgrammer can't see network disk

I've just noticed that STM32CubeProgrammer (2.19.0) can't see network disk on my Windows 10 PC.I have also set a folder inside of one of the network disk as favourite folder to rapid access on the left sidebar but, when I click it via STM32CubeProgra...

nico23_0-1741615285777.png
nico23 by Senior III
  • 1500 Views
  • 4 replies
  • 0 kudos

Resolved! How to verify internal flash content without changing RDP

STM32f334 在Stm32cube programmer中如何不改變RDP的情況下,驗證MCU內部程式為正確的,透過找出沒有被RDP1鎖住的FLASH去驗證,或是如何透過改寫OB來驗證?Translation:How to verify the correctness of the internal program of STM32f334 MCU in Stm32cube programmer without changing RDP, by finding the FLASH that...

eeee9797 by Associate
  • 1103 Views
  • 1 replies
  • 1 kudos

Resolved! Licensing of STM32Cube USB Drivers

Hello,I am working on a project where a device is updated using dfu-util and utilizes the DFU driver from the STM32Cube(Programmer) drivers subdirectory. I would like to distribute these drivers to my customers and need to know, for the FOSS Software...

Bengr by Associate
  • 1434 Views
  • 1 replies
  • 2 kudos