STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! cubeprogrammer can not find masserase function

I created an external flash STLDR file for my board, with STM32H750VB chip and W25Q64 QSPI FLASH. After copying the STLDR file to the cubeprographer directory, it can perform normal external flash read/write and sector erase functions. However, when ...

Resolved! Thanks for Incremental Flash

Hi,Many thanks for the experimental incremental flash feature! For me it speeds up the dev cycle considerably.  (Note https://wiki.st.com/stm32mcu/wiki/STM32CubeProgrammer_errata_2.21.x seems to be broken.)Dan 

codebuk by Associate III
  • 497 Views
  • 2 replies
  • 5 kudos

STM32CubeProgrammer

I have a problem with installing STM32CubeProgrammer. The installion of this program has 9 steps. However, I cannot see step 8 and step 9. For this reason, I cannot install the program. When I am looking for the solution, some people say that compute...

user1235_0-1760862572069.png
user1235 by Associate
  • 3931 Views
  • 1 replies
  • 0 kudos

Resolved! firmware uploading with FT232RNL IC to F413

I am having some issues with getting UART uploading working. I can read the chip and get it's ID, but it keeps saying it cannot get acknowledgments.  Everything is directly connected. Serial TX/RX to their corresponding pins and RTS to Boot and DTR t...

AndrewC_0-1759943267505.png
Andrew C by Associate III
  • 1538 Views
  • 11 replies
  • 0 kudos