2024-11-07 1:53 AM - last edited on 2024-11-07 1:57 AM by Andrew Neil
Without starting the STM32 Cube Programmer (GUI) I get following error message:
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.31V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
Done
After I have started the STM32 Cube Programmer it works:
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
JTAG freq : 21333 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x483
Revision ID : Rev Z
Device name : STM32H72x/STM32H73x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x93
Hard reset is performed
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
JTAG freq : 21333 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x483
Revision ID : Rev Z
Device name : STM32H72x/STM32H73x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x93
Mass erase ...
Mass erase successfully achieved
Done
The problem can be reproduced by disconnect the STLINK V3MINIE.
I am using the latest version: V2.17.0
In my boundary scan test environment I need the command line programming.
Does anyone have an idea?
Many thanks in advance
Joerg
2024-11-07 5:08 AM
show the command line you are using
2024-11-07 6:33 AM
@Echo OFF
SET TOOL="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe"
ECHO Press ENTER to erase chip
pause
%TOOL% -c port=JTAG -hardRst
%TOOL% -c port=JTAG reset=SWrst -e all
ECHO Done
pause
2024-11-07 6:41 AM
First, try running it with Echo ON - to ensure that your variable is getting properly expanded.
What happens if you explicitly specify your target MCU on the command line?
2024-11-07 7:23 AM
Hello Andrew,
Many thanks for your help.
I didn't found any parameter to set the MCU in the command line.
2025-01-23 9:54 PM
The only way at the moment is, to start one times the GUI before you are using the CLI tool. In my boundary scan environment I start the GUI at the beginning and kill the process 10s later. This is a workaround but no solution. I hope ST will fix this problem in the future.