STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Different drivers DfuSe Demo vs. STM32CubeProgrammer

In order to see my microcontroller (G4 series) listed as Dfu device inside STM32CubeProgrammer the USB driver inside windows has to be of type "STM32 Bootloader"But to see it appear inside DfuSE Demo, the USB driver has to be of type "STM Device in D...

WSpar.1 by Associate III
  • 1399 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeProgrammer is now the only way to program most of the newer STM32 uControllers. Has anyone been able to get it to work on Windows 10 with OpenJDK 8? I've spent a lot of time on it with no luck.

Given that Oracle has changed their Java license to a commercial license that many developers and companies will be reluctant to accept, the dependency of STM32CubeProgrammer on it is problematic. Although the documentation suggests that it will work...

_dalbert by Associate III
  • 6250 Views
  • 12 replies
  • 2 kudos

Resolved! Verification progress bar bugged?

When using the command line version of STM32CubeProgrammer, I notice during the verification process (-v flag), the progress bar follows a sequence like 6%->12%->18%->24%-18%->24%... and ends at 24%, with a successful verification. Picture provided f...

0690X00000Bw3eTQAR.png
jefflongo by Associate III
  • 6578 Views
  • 13 replies
  • 0 kudos

Update Firmaware wrongly

I updated my tilebox firmware usisg STMCubeProgrammer. I updated the worng firmware version, and now my tilebox doesn't work and I doens't switch on. Is there any way of restoring the original firmaware?

NMart.1 by Associate III
  • 1853 Views
  • 4 replies
  • 0 kudos