User Activity

When you place the STM32L471 in DFU mode and attempt to connect via UART, the following is displayed in STM32CubeProgrammer:14:39:27 : STM32CubeProgrammer API v2.5.014:39:28 : Serial Port COM9 is successfully opened.14:39:28 : Port configuration: par...
Given that Oracle has changed their Java license to a commercial license that many developers and companies will be reluctant to accept, the dependency of STM32CubeProgrammer on it is problematic. Although the documentation suggests that it will work...
Posted on October 11, 2016 at 21:00Using an STM32L051, I am unable to generate a 32MHz system clock from from the PLL using the HSI as the clock source.  I can generate up to 24MHz without trouble, but any attempt to generate higher frequencies resu...
Kudos from