STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Hot to update STM32F4DISCOVERY BOARD ST-LINK?

I did some AI examples at the STM32F4Disco Board. After that Cubeprog. doesn't connect to discoboard.When I connect the discoboard to my PC with usb, PC recognize the board but Cubeprog. doesn't connect to board.Error code is given below.12:45:29 : ...

Ogünd.1 by Associate
  • 1145 Views
  • 1 replies
  • 0 kudos

STM32H747 Dual Core Programming Both Cores

I have an application built in CubeIDE that utilizes both cores on the H747I-Disc1 board. The M4 core collects data and uses HSEM to notify the M7 core to process it. In debug mode I can run this just fine by first launching the M7, letting it run an...

RDock by Associate II
  • 4885 Views
  • 5 replies
  • 0 kudos

STM32CubeProgrammer - Bug report - External Loaders

Hello,Please move this to a more appropriate section if required, or let me know if there is a better way to report bugs.I have come across a couple of bugs whilst developing an STLDR for external flash access, note the memory arrangement of the flas...

0693W000000VN9wQAG.png
JHedges by Associate III
  • 3186 Views
  • 6 replies
  • 0 kudos

DFU status response for STM32CubeProg

Hi,I've create my own bootloader with USB DFU functionality. (I need some function that built-in bootloader can't provide)I'm able to read/write/erase application firmware by USB DFU now.however, I find the STM32CubeProg work differently with built-i...

JWu.2 by Associate II
  • 2394 Views
  • 4 replies
  • 0 kudos

Resolved! programming a cortex-m0+ (STM32L073RB) device with a hex-file that uses not the whole memory or has leaks leads to wrong initial byte in flash memory of device

Hi everybody,I use the STM32CubeProgrammer version 2.3.0Following issue occurs during programming of a hex-file:1.) do a mass-erase or a clear of all sectors of the device2.) read out some bytes (for example the first sector)3.) the device-memory tab...

0693W000000WYiQQAW.png 0693W000000WYh8QAG.png 0693W000000WYhNQAW.png 0693W000000WYh3QAG.png
BNest.1 by Associate
  • 2340 Views
  • 4 replies
  • 1 kudos

How uncheck Option byte ?

I used STM32G070. According to the reference manual RM0454 rev2, it does not exist in this procesor Option byte IRHEN (in User Configuration). But the program allows you to set it.I did it, the processor stopped working, and no Option byte can now be...

Peko by Associate III
  • 2863 Views
  • 6 replies
  • 0 kudos