STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer-Windows OS

Hello, DFU is not working in STM32Cube Programmer, I can see the connected board in device manager under universal serial bus controllers, please your advise.Thanks

AAmer.1 by Associate II
  • 6392 Views
  • 11 replies
  • 0 kudos

STM32Cube programmer

Hello, I'm trying to install STM32CubeProgrammer on linux -ubunto, I applied sudo SetupSTM32CubeProgrammer-2.4.0.linux, and the installation process started, and I got app on desktop, but its not working, when I click on the icon the installation p...

AAmer.1 by Associate II
  • 985 Views
  • 1 replies
  • 0 kudos

Resolved! Hi. I have enabled PCROP protection in STM32CubeProgrammer and would like to disable it now. How do I disable it?

When I tried to do it in STM32CubeProgrammer I receive the next error:18:37:09 : OPTION BYTE PROGRAMMING VERIFICATION:18:37:09 : Error: Expected value for Option Byte "SPRMOD": 0x0, found: 0x118:37:09 : Error: Option Byte Programming failed

OKuro.1 by Associate II
  • 3367 Views
  • 3 replies
  • 0 kudos

Resolved! Error: No STM32 target found in STM32CubeProgrammer

Hi guys, I disabled flashing core M7 in STM32CubeProgrammer option bytes to run just M4, but now I cant connect to the board and the tool says Error: No STM32 target found!. Is there some possibility how to reset the option bytes to again run M7?Than...

binarybee by Associate III
  • 4144 Views
  • 8 replies
  • 0 kudos

Fail during download with bootloader in USB DFU mode

I have a custom board with a STM32H743ZI 144-pin processor. I can start the bootloader and the device is correctly recognized in the STM32CubeProgrammer as DFU in FS mode. I can read from device memory without issue, however when I try to download a ...

0693W000000WK1mQAG.png 0693W000000WK4lQAG.png
MLovr.1 by Associate II
  • 3546 Views
  • 5 replies
  • 0 kudos