cancel
Showing results for 
Search instead for 
Did you mean: 

Can not program STM32F7NI_Discovery, because i enabled the Read Out Protection level 2 (by mistake)

Abdou
Associate II

Hello,

I have problem with a custom STM32f769_Disc based board. It was working nomal and i activarte the Read Out Protection level 2 (ROP by mistake) from ST-Link, and the st-link stopped working and i can't program it anymore From IAR / St-Link /STM32CubeProgrammer .

How can i Disable Read Out Protection (level 2) ??????.

Please help.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

>>How can i Disable Read Out Protection (level 2) ??????

You can't, that's the whole point.

ONCE AND DONE!

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Abdou
Associate II

thank you for your answer,

soo what have i do now ???

how i can program it again ??

Andreas Bolsch
Lead II

Clive's answer was clear enough, wasn'it? Check the corresponding RM.

Your board is for the bin now (given that the program present in the flash doesn't suit your needs).

Reposting the response to PM

You've permanently broken it, it is not recoverable.

Normally you have software on the board you want to protect, and that software would provide alternate means of interaction. Usually this would be a loader which is never erased, but allows for secure updates of other application code.

Perhaps you know someone locally who can remove and replace the STM32 IC on the board?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..