cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer-Windows OS

AAmer.1
Associate II

Hello,

DFU is not working in STM32Cube Programmer, I can see the connected board in device manager under universal serial bus controllers, please your advise.

Thanks

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
TDK
Guru

Does it show up in device manager as a DFU device? Show a screenshot. It's not in that mode by default, you need to start the bootloader with USB enabled and nothing else talking to the chip.

If you feel a post has answered your question, please click "Accept as Solution".

Hello @AAmer.1​ 

which board do you use ?

Best regards,

Nesrine

Hello Nesrine,

I have our own board.

BR

Hello @AAmer.1​ 

So, it is necessary to know if your Board contains a bootloader or not.

Best regards,

Nesrine

this is the reason why I'm trying to connect to it, I need to flash it with bootloader.

It is necessary to check the boot on the system memory.

yes I knew, the boot are correct, strange.

No it appears as USB serial converter

Hello @AAmer.1​ 

I think that the problem is on the user's own board not on the Cubeprogrammer.

Best regards,

Nesrine