STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Wont launch on Mac 10.15.6, binary improperly signed.

First off I am running java 8:java version "1.8.0_261"Java(TM) SE Runtime Environment (build 1.8.0_261-b12)Java HotSpot(TM) 64-Bit Server VM (build 25.261-b12, mixed mode)Ive tried installing this software two different ways:java -jar SetupSTM32CubeP...

Js.1 by Associate
  • 827 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer fail to connect over DFU

Hello,When I try to connec to my STM32H743 micro using USB in DFU mode , it fails and gives the following message13:27:11 : STM32CubeProgrammer API v2.5.0 13:27:31:738 : Device Descriptor: 13:27:31:739 : |_bLength : 0x12 13:27:31:739 : |_bDescriptorT...

HAlzo by Senior
  • 890 Views
  • 0 replies
  • 0 kudos

Resolved! STM32CubeProgrammer "Unable to list supported devices"

I'm trying to use STM32CubeProgrammer on a Ubuntu system to read and eventually write the flash on my STM32F030 device via an ST-Link. However when I click the 'Read' button, after connecting to the ST-Link I get two errors: Error: Unable to list su...

DTovey by Associate II
  • 3788 Views
  • 2 replies
  • 0 kudos