STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32VLDISCOVERY (DEVICE_NOT_SUPPORTED)

Hello,I am using Ubuntu 18.04 LTS and CLI version of STM32CubeProgrammer 2.5.0.My board is STM32VLDISCOVERY with STM32F100RBT6 MCU. When I do list devices or connect, I get DEVICE_NOT_SUPPORTED. Attaching log.Thanks,Mitul

MMeva.1 by Associate II
  • 2612 Views
  • 4 replies
  • 0 kudos

STM32L562E-DK Failed to connect.

Hello STM team,I am working with STM32L562E-DK. It was working fine, but suddenly the STM32L562E-DK is failing to connect. And generates a FAIL.TXT which says "The interface firmware FAILED to reset/halt the target MCU".NOTE: I have not done any modi...

Neel by Associate III
  • 1398 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer 2.5.0 released

New features • Added the support for STM32G491xC and STM32G491xE microcontrollers • Added the support for STM32H72xxx and STM32H73xxx microcontrollers • Added SFI support for STM32H72xxx and STM32H73xxx microcontrollers • Added SFIx support for STM32...

Detects wrong device and and cannot program

I am trying to program a generic STM32L151C8T6A via STlinkv2 If I use STM#@ ST-LINK Utility I have no issues and this is what it detects:14:56:17 : Device ID:0x429 14:56:17 : Device flash Size : 64KBytes14:56:17 : Device family :STM32L100x6xxA/L15xx6...

0693W000003RtsdQAC.png 0693W000003RtsiQAC.png
AToog.1 by Associate II
  • 2110 Views
  • 2 replies
  • 0 kudos