STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Stm32 code reading

I have a Stm32 which was coded by my friend. I want to reach this code and I want to change some thing. How can I do it.(note: code doesnt have reading protection)

ÖÇoba.1 by Associate II
  • 3018 Views
  • 5 replies
  • 0 kudos

Run after the programming option doesn't work

I'm using STMCubeProgrammer for program STM32F103 MCU. But I don't have any access to MCU RESET PIN. So I enter to BOOT Mode by source code in my application, But when I want to turn back to application from boot mode the "Run After Programming" opti...

HKaze.1 by Associate
  • 1150 Views
  • 1 replies
  • 0 kudos

Using Multiple ST-Links on the command line interface

I am building an application which will program 4 STM32G030 mounted on built PCBs in a test rig but cannot work out how to use 4 ST-Links connected to a USB hub in my test rig to do this. I need to run the ST-Links in parallel, not sequentially, to s...

AEmer.2 by Associate II
  • 4793 Views
  • 5 replies
  • 0 kudos

Stm32cubeprogrammer

Hi,​I just got a PCB with integrated stm32f0... Chip, which can be flash though ISP,usart, UART, Swd..​​But I downloaded the stm32cubeprogrammer to flash the chip as the hex and bin file was sent to me I keep getting the error o the bootloader stuff,...

AAkin.1 by Associate II
  • 5042 Views
  • 9 replies
  • 0 kudos

Resolved! [STM32H750] Can not upgrade the firmware by STM32CubeProgrammer when I have used the DTCMRAM section

[STM32H750]  Can not upgrade the firmware by STM32CubeProgrammer when I have used the DTCMRAM sectionjust add this code : the STM32CubeProgrammer will upgrade failed:​__attribute__((section(".DTCMRAM"))) uint8_t buf[2400] = {0};​int main(void){xxxx....

Davi by Associate II
  • 1421 Views
  • 1 replies
  • 0 kudos