cancel
Showing results for 
Search instead for 
Did you mean: 

Can I install STM32CubeProgrammer on my linux machine

AĆosi.1
Associate

Hello,

My Linux specs:

  • Linux lime2 3.4.104-00136-gd47d367
  • armv7l GNU/Linux

SetupSTM32CubeProgrammer.linux file's information:

  • ELF 32-bit LSB executable
  • Intel 80386
  • version 1 (GNU/Linux)
  • for GNU/Linux 2.6.24
  • not stripped

When I try to install, error shows up saying that installation couldn't create folder /bin/ and temporary file "libstp11_SAM.so.conf".

When I manually add mentioned file and folder, installation finishes but I cannot run "STM32CubeProgrammer.desktop" file which is created on my desktop.

So, my question is whether I can install CubeProgrammer on my machine based on given specifications?

Thanks in advance,

A.C.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Houda GHABRI
ST Employee

Hi @ACosi.1,

Sorry for the late reply.

I need more in formations, can you please follow these steps and send me the traces:

-go to CubeProgrammer install folder\bin

-launch CubeProgrammer CLI : java -jar STM32CUbeProgrammer_CLI.exe

=> send me the traces in cmd.

regards,

Houda