STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! No OptionByte setting from file

I am trying to migrate from UM0462 Flash Loader Demonstrator to the STM32CubeProgrammer (upon a recommendation from STM, as the former becomes obsolete). Yet I seem to be missing the option of loading OptionByte file.The documentation for cube refers...

0693W000005CCnsQAG.jpg
DarkLight by Associate II
  • 2240 Views
  • 4 replies
  • 0 kudos

STM32FG031 once pin 4 (PF0 - NRST) is set as GPIO input, it is not possible to reprogram the MCU flash. How to recover ?

Working with a STM32G0316-DISCO, I was so stupid I wrote a test program where I set pin 4 (NRST) as GPIO input (PA0). It goes without saying that now I'm not able to reprogram che MCU. Is there any magic trick to get out of this situation aside buyin...

Frabs by Associate II
  • 2585 Views
  • 6 replies
  • 0 kudos

Run target on STM32H747I-DISCO failed

please refer to this..https://community.st.com/s/question/0D53W00000O1KHJSA3/run-target-on-stm32h747idisco-failedwhen I use 2.5.0 i get thisRun Target Generate Wrote generated/gui_generated/src/main_screen/MainViewBase.cpp Done ...

Resolved! STM32CubeProgrammer reports no STM32 target found.

I'm using the P-NUCLEO-STM32WB55 board and programming was working, but it stopped. I didn't change any jumpers, etc. I'm using a USB cable from PC to the ST-LINK connector. The last firmware successfully programmed was the BLE_TransparentMode exa...

JTomp.1 by Associate II
  • 1512 Views
  • 2 replies
  • 0 kudos