STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

SWV Console Automated

Hi there,I've an issue when trying to automatize the SWV command with Jenkins. The issue is that when I run the command: STM32_Programmer_CLI -c port=SWD -swv freq=216 portnumber=0 it asks the user to press 'R' in order to start. Since Jenkins has no...

0693W000007ZqaKQAS.jpg
RCast.2 by Associate
  • 1690 Views
  • 3 replies
  • 1 kudos

Problem Erasing Chip Memory - Read Out Protection

Hello everyone!I work with a Nucleo board F446RE. One month ago i lended my board to one of my university collegue. After a while he gave me back my board, but i can't use it anymore. When I try to flash a program with STM32Cube IDE it gives me an er...

RHuzy.1 by Associate II
  • 3304 Views
  • 6 replies
  • 0 kudos

Resolved! SWD connection no longer working

Hello,On a STM32L4 design, we no longer have an SWD connection to the processor: using STM32CubeProgrammer reports ST-LINK SN : 39FF6A064243383912381057ST-LINK FW : V2J36S7Voltage : 3.26VSWD freq : 4000 KHzConnect mode: NormalReset mode : Software re...

RHaag.1 by Associate II
  • 5783 Views
  • 13 replies
  • 0 kudos

STM32F030C8T6> connect with STLINKv2 & STCube Programmer..... I want to flash firmware using SWO port. Pin connections are TVCC(pin1), SWCLK(9), SWIO(7), STM32rst(15) GND(12).

 Error: No STM32 target found! This is the CONSTANT message I get from the STCUBE software. I can see reference voltage from my board but actually connecting to the chip is impossible  Error: No STM32 target found!,  Error: No STM32 target found!, Er...

AHolm.1 by Associate
  • 2149 Views
  • 2 replies
  • 0 kudos

No ST-LINK detected in STM32CubeProgrammer

Hi,I'm having some trouble with getting my (genuine) ST-LINK v2 detected in the STM32CubeProgrammer. The strange thing is, the STM32CubeIDE and also the firmware update utility detect the ST-LINK v2 without any issues. Already tried different USB por...

0693W000007ZGORQA4.png
HGreg.1 by Associate II
  • 1967 Views
  • 5 replies
  • 1 kudos

Flashing stm32h7b3-dk issue,

 I am trying to restore the demo file that came with this discovery kit. Erase all works but when I try to program it I get these errors after the erase is complete: 17:48:08 : Download in Progress: 17:48:11 : Error: failed to download Segment[9] 17:...

JWalt.1 by Associate II
  • 2054 Views
  • 4 replies
  • 0 kudos