cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer error message !

MYu.1
Associate II

I use STM32CubeProgrammer, but i can't use STME2CubeProgreammer

I try to connect it to board, but error message happen.

below error message.

07:02:43 : ST-LINK SN : 066DFF383337554E43123655

07:02:43 : ST-LINK FW : V2J37M27

07:02:43 : Board    : NUCLEO-G070RB

07:02:43 : Voltage   : 3.22V

07:02:43 : Error: No STM32 target found!

i already did frimware upgrrade

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
DavidAlfa
Senior II

Assuming the connection is correct, I guess you didn't enable SWD.

If you didn't enable the SWD interface in the firmware, It will be disabled after booting, the programmer won't be able to connect unless you use nRST pin, or manually hold nRST low before clicking on Program, and then release.

The manual method requires some tries until getting the correct timming​