STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32F410 EXTERNAL LOADER CREATE

Good morningI am trying to create and use SPI EXTERNAL LOADER using STM32F410 CBT3. I created EXTERNAL LOADER using S25FL032P_STM32G071B_NUCLEO sent from STM. Data is read from STM32CUBEPROGRAMMER, but data mismatch found at address 0x90000000 occurs...

GGIL.1 by Associate II
  • 1350 Views
  • 1 replies
  • 0 kudos

Resolved! External Loader with STM32CubeProgrammer

I created an external loader, I tried it with STM32CubeProgrammer. Most of the time its not working, rarely it can read the data and erase. When it happens I am trying to program the memory and it can program ~400 KB then it fails. Then I used ST-Li...

kb24 by Senior
  • 3423 Views
  • 2 replies
  • 0 kudos

Resolved! STMCubeProgrammer will not start

I just installed en.stm32cubeprg-win64_v2-7-0.zip.Installation went without problems but when I try to start the application I get the splash screen and then it just exits apparently. If I runt it from a prompt I get no messages.C:\Program Files\STMi...

Setting Auto mode with STM32CubeProgrammer v2.7.0

I have just started using STM32CubeProgrammer v2.7.0 and I liked the simple and great looking UI over the other programmers. Now I would like to use Automatic mode and expect the following:Erase the Read Out Protection (RDP) in OB or set it to "AA"Fu...

JABRA.1 by Associate II
  • 5404 Views
  • 9 replies
  • 0 kudos

FDCAN programming support?

As far as I can tell, cube programmer supports programming over CAN, but not FDCAN, like on the newest MCUs. True? Is there a path for STLink and cube programmer to support FDCAN?

MMedv by Associate II
  • 1693 Views
  • 1 replies
  • 0 kudos

Programming via UART

Hello,I am trying to program Nucleo- H743ZI2 via UART (UART3) according to AN2606 doc page 244.I have managed to successfully program small bin and elf files. However, when I try to program a bigger file (bin = 655,619KB, elf = 5870KB) I am getting a...

IShar.2 by Associate II
  • 759 Views
  • 0 replies
  • 0 kudos

STM32 QSPI external flash loader issue

Hi.In a project I'm working on, I have to use external flash because the internal flash memory is low.I decided to use the MT25QU512ABB chip as it supports QSPI. After some research on the internet, I found the video of STMicroelectronics on youtube ...

johnLocke by Associate II
  • 3869 Views
  • 5 replies
  • 0 kudos