STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

SWV Hex Display

Is it possible to display the data from the ITM over the SWV viewer (NUCLEO-F401RE) in STM32CubeProgrammer in HEX? ITM_SendChar could be used to send just a 32-bit code, which takes far less CPU time than a printf-style debug output?

Amigo by Associate III
  • 782 Views
  • 0 replies
  • 0 kudos

STM32L152VD-X reserved memory space

Hello,I am using the STM32CubeProgrammer, version 2.10.0, and it does not detect the STM32L152VD-X reserved memory space, at address 0x0803000.The STM32CubeProgrammer detects the correct device ID which is 0x437 but does not detect the correct device...

VLock.2 by Associate
  • 3211 Views
  • 4 replies
  • 0 kudos

After the stm32g0xx chip is set to read protection level 1, the protection level can no longer be set to 0.

The method is as follows:1. First, set the flash option byte to force boot from the main flash.2. Set the read protection level to level 1.After this setting, the st-link tool will no longer be able to connect to the chip, which is equivalent to losi...

victor.wu by Associate II
  • 1108 Views
  • 1 replies
  • 0 kudos

Embedding option bytes in hex file

Hi all,The goal is to embed option bytes in hexfile, such that when production are doing their thing, the correct settings are automagically selected.But stm32cubeprogrammer fails with:Error: Data mismatch found at address 0x1FFF781B (byte = 0x00 ins...

nonesuch by Associate
  • 2124 Views
  • 1 replies
  • 1 kudos

Retrieve MCU Device ID from USB DFU

We are working on our own firmware update utility, and need a way to get the Device Id from default USB DFU bootloader in order to avoid wrong firmware flashing. On CubeProgrammer, we can see that info: 21:36:20 : Device ID  : 0x0423The question is: ...

NChin.2 by Associate II
  • 2551 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer 2.10.0 does not work on Linux

Hi,I tried to install STM32CubeProgrammer v2.10.0 on my Kubuntu 20.04.4.The error I get is CubeProgrammer_API or one of its dependencies is missing.What I could find from the forum is that could mean the installer used a different Java/OpenJDK versio...

Arno1 by Senior
  • 1437 Views
  • 1 replies
  • 0 kudos