I have managed to use the CubeProgrammer_API.dll in a visual studio C# project. Everything seems to be working properly but when I try to set the verbosity level nothing changes. It seems to be fixed to level 2. This is the code I'm using:[DllImport(...
Hello,I am using the STM32L412, when I activate the HSI clock in the .ioc, HSI Calibration Value is set to 16 (0x10).Looking at stm32l4xx_hal_rcc.h:#if defined(RCC_ICSCR_HSITRIM_6)
#define RCC_HSICALIBRATION_DEFAULT 0x40U /*!< Default HSI ca...
Ups you are right, I've created a new test project with the same target and it is set to 0x40 by default. I don't know what could had happen with the other project.Thanks for the response