User Activity

Hello,my CPU is a STM32H745. I want to flash data into both banks (bank 1, sector 2-7, complete bank 2, while the code runs from the first bank, sector 0+1.I'm using the given HAL-drivers stm32h7xx_hal_flash.c and stm32h7xx_hal_flash_ex.c and found a...
Hello , maybe I post this question to the wrong place...I would like to use ST-LINK/V2, Part number for required Software is "STSW-LINK009".In the description I can read "driver signed for Windows7, Windows8, Windows10".Could someone confirm that thi...
Hello, I used CubeProgrammer 2.7.0 to get infos about a board with STM32F??? (device marking on the chip not completely readable)I enabled the checkbox "Read Unprotect", the documentation says it is "changing the RDP level from level 1 to level 0".Af...
Hello, I try to programm a STM32F765 via USART1 (PA9/PA10), but the connection fails. I use STM32CubeProgrammer v2.7.0.If I use USART3 instead on my target, programming works as expected.Q: Is there a known bug, and USART1 does not work on this CPU? ...
Hello,can we integrate an STLINK debug interface into our module? The module uses an STM32F7xx.If yes, where would I find related documents (example schematic, BOM, firmware) ? This would allow our customers to update the firmware and debug their ow...