STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Debug autentification with certificate on STM32H563

Hi. How can i connect a debug session to a device with product-state: closed and non secure software (no TZ active) without full regression.   I have create the password.bin file and two certificate files with TrustZone Package Creator: - DA with p...

stm32cubeide_rV2jj6lTVp.jpg

Resolved! STM32F4 [X-CUBE-CRYPTOLIB] - Cryptography Support

Hello,I am using the Nucleo-STM32F411RE development board and require support for cryptographic functions, particularly ECC NIST P-256, MAC, etc, for my development use cases.To achieve this, I downloaded the X-CUBE-CRYPTOLIB v4.3.0 package as it was...

Akash_M by Associate II
  • 2752 Views
  • 3 replies
  • 0 kudos

Resolved! Failed to provision Secure Manager 1.2

I tried to provision Secure Manager 1.2 to my DK board, and got the following error messages in the provisioning.log:2024-11-10 15:49:30,796 - root - DEBUG - Error: SFI command is not supported for the current device configuration using STLINK interf...

Thatseasy by Associate III
  • 4741 Views
  • 11 replies
  • 1 kudos

Problem with UART in secure and unprivileged mode U5

I am encountering an issue in the development of the TrustZone application related to the UART in secure non-privileged mode.I want to switch to non-privileged mode when in secure and privileged mode. This transition works correctly. However, I have ...

ECoud.1 by Associate III
  • 2351 Views
  • 3 replies
  • 0 kudos