cancel
Showing results for 
Search instead for 
Did you mean: 

SBSFU intrusion

Istillaga
Senior

Hi

I'm using the SBSFU example for the STM32U5 microcontroller. After an intrusion, the board enters a locked state. Is there a way to receive a notification when an intrusion occurs and another when it has ceased, indicating that the board can return to its original state?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bubbles
ST Employee

Hi @Istillaga,

for the intrusion mechanism explanation it's best to go to the RM0456 reference manual. You see that the intrusion is described in the Flash memory section, starting from chapter 7.6.2. There's nothing to configure about it. It's linked to the RDP level and protects the SW from readout attempts.

Only way to leave the intrusion state is reset.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.