STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can we load .bin file in place of .elf file for debug purposes in the system workbench for stm32 , I do not need break points , I know I can load the same file using j_flash utility but I want this process with system workbench

At the debug mode I would not like to provide .elf file , as the generated elf file does not have CRC that is generated .In STM system workbench I use post build command to generate .bin file and than I use srec-cat script to generate CRC on this .b...

My question is about intellectual property theft at CMs. Clearly ST recognizes the issue and even addresses it by adding SFI (secure internal firmware install) on some microcontrollers. AN5054 is listed in the resources for STM32L010K4; however, it is my

My question is about intellectual property theft at CMs. Clearly ST recognizes the issue and even addresses it by adding SFI (secure internal firmware install) on some microcontrollers. AN5054 is listed in the resources for STM32L010K4; however, it i...

KMalt.1 by Associate II
  • 2776 Views
  • 7 replies
  • 0 kudos

meeting on 2nd Juliy didn't start / can't join

in my invitation it's said, that the introduction starts at 8:30I can't join (8:50) and get following message:Sobald die Besprechung beginnt, geben wir den Personen Bescheid, dass Sie warten.Wenn Sie der Organisator sind oder die Einladung von Ihrer ...

CAmbe.1 by Associate II
  • 1328 Views
  • 3 replies
  • 0 kudos

I have not yet received the boards

Hello,I have not received yet the board. Can I join in the workshop anyway? Why did you send the email for filling the form only 2 days before the workshop?

Lorig.1 by Associate
  • 914 Views
  • 2 replies
  • 0 kudos

Once in the system bootloader, is there a way to update a readout protected firmware with only an UART access (and no BOOT0 access)?

Hello,Objective:I have to update the firmware of an STM32F412 using the bootloader in system memory (through UART protocol).Situation:A command in my user code allows jumping to the bootloader after a system reset (so the device is in nominal state)....

PA:99 by Associate II
  • 1915 Views
  • 4 replies
  • 0 kudos