User Activity

Dear support team, can I run both outputs of the VND5004ATR-E parallel to decrease the RDSon even more? So just connect both inputs and the load on both outputs? Thanks
As in https://community.st.com/t5/power-management/vn5050aj-cs-dis-not-working/m-p/632201#M10745 we now have added seriel diodes for every chip, but it is still not disabling his Current_Sense Output altough the CS_DIS Pin is above 3V.  The CS_DIS-1 ...
We have a new design were we have multiple VN5050AJ high side drivers. We have connected all current sense pins together and want to enable just one current sense per time to save analog inputs. Now it seems that the CS_DIS pin is ignored and the chi...
We have multiple VND5160AJ-E on a new product were we use every single channel as an output channel. Some outputs should driver 4 Ampere which would be perfect doable if we run both channels in a chip parallel. So are the any concerns about doing thi...