xray format issue
STD120N4F6 dc 20+ , found that the xray format is difference from DC 21+, did there a new PCN during 20+ i'm not sure if these goods are origin. could you pls help to check the labels for me?
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
STD120N4F6 dc 20+ , found that the xray format is difference from DC 21+, did there a new PCN during 20+ i'm not sure if these goods are origin. could you pls help to check the labels for me?
Hello everybodyI'm using a custom board in which there's a STM32F030 that communicate with SPBTLE_RF0 module. With X-CUBE I generate software using X-CUBE-BLE2.2.0.0.I can reset the chip and read response (vendor specific event), but when I try to co...
Hi,I picked up a X-NUCLEO-BNRG2A1 (Extension board Lot:2040 for the Nucleo-64 boards), and I am trying to communicate with it through a Nucleo-F411RE Board. I basically generated a project template through CubeMX for the STM32F411RE and included the ...
Hello. I have flashed DTM_UART firmware to my BlueNRG device. I have connected RX/TX pins to IO8/IO11 of the BlueRNG but when I start the device, on serial monitor I only see: and cannot open the device via BlueNRG-GUI.I have picked up the binary fil...
I would like to experiment with BlueNRG FW. I have downloaded BlueNRG SDK from:https://www.st.com/en/embedded-software/stsw-bluenrg1-dk.htmlAnd also I have recently downloaded Wise Studio that I would like to use for building BlueNRG code.In the Wise...
Hi,I'm using BLE_SensorDemo project. I have created my own services. Everything works fine reading and writing the data. The only problem is, when I try to connect from my Android mobile, I could not connect to to the BlueNRG-2 in first attempt. I ha...
I copied the code snippet and vtimer.c from RTC_Virtual_Timer project to BLE_Beacon project. But HAL_VTimerStart_ms always returns 0x01 error(=timer already started). Similarly, I copied the same code to Micro_Sleep_Test project, it works normally wi...
hello ,I try to use USB1602 chip build an PD Triger based STM32F103ZE , I download STSW-STUSB010-V1.0.1 and build all the target using MB1303_SINK_ONLY project. I cannot find USBPD_PE_Init(.....) function and some other function defin...
Dear all,I am currently evaluation the BlueNRG-LP for a new project. I am using the STEVAL-IDB011V1 board and BLE stack v3.1. I've started with the BLESensorDemo to implement our own service. My question is regarding the BLE address.This is how it is...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.