User Activity

I am a bit confused about the number of connections the BlueNRG-LP can handle.The device is advertised with 128 concurrent links.I visited a ST talk where the discussed number was about 50 Connections.I used the BlueNRG-LP 1.0.0 Radio Wizard that lim...
My evalboard seems to work. (I can flash the demo projects)But when I try to use the GUI, it does not detect the device. "No Firmware detected on motherboard..."It is successful to flash the Firmware STEVAL-IDB011V1/USB_CMSISDAP.hex but afterwards e...