cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to connect to hidden wireless network with SPWF01SA21 on FW3.4

ballenstorfer
Associate
Posted on September 15, 2015 at 12:44

Hi,

I tried to connect to a wireless network, which do not broadcast its SSID, with the above mentioned module.

I tried as usual:

AT+S.SCAN

AT+S.SSIDTXT=TestAP

AT+S.SCFG=wifi_wpa_psk_text,Test123

AT+S.SCFG=wifi_priv_mode,2

AT+S.SCFG=wifi_mode,1

AT&W

AT+CFUN=1

The response after the reset is just the scanning procedure...

+WIND:2:Reset

+WIND:1:Poweron (150410-c2e37a3-SPWF02S)

+WIND:13:ST SPWF01SA2 IWM: Copyright (c) 2012-2014 STMicroelectronics...

+WIND:3:Watchdog Running

+WIND:46:WPA: Crunching PSK...

+WIND:0:Console active

+WIND:32:WiFi Hardware Started

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete (0x0)

Is there something I've to add to the configuration to get it done?

Thanks
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Gerardo GALLUCCI
ST Employee
Posted on September 15, 2015 at 17:42

Hi Joe,

Config is ok.

I raised your issue. Give me a couple of days...

Thanks

jerry

Gerardo GALLUCCI
ST Employee
Posted on September 17, 2015 at 14:27

Hi Joe,

problem was confirmed. It will be solved into next FW Release.

Thanks

jerry

Gerardo GALLUCCI
ST Employee
Posted on September 17, 2015 at 14:28

Hi Joe,

problem was confirmed. It will be solved into next FW Release.

Thanks

jerry